We put all our passion for technology into developing the best solutions for our customers. Do you need advice about a specific application?

Contact us now
Customer: NewCold

Location:
Breda, Netherlands

Sector:
Service provider for cold storage logistics

Application:
Shuttles, storage/retrieval systems, pallet transfer shuttles, rail guided vehicle, hoists and conveyors

Contact form Worldwide locations Contact information

By activating the zip code search, data is transferred to the USA by Google. For more information, see our privacy policy.

Facility Operator NewCold:

  • The company has a global network with 11 locations on three continents. In total, NewCold offers over 927,000 pallet spaces.
  • Headquarters: Breda, Netherlands
  • Industry: Deep-freeze logistics service provider
  • Number of employees: 1,200
  • Project location: Rennes, France
  • Applications in the project: Shuttles, storage/retrieval systems, pallet transfer shuttles, electric monorails, vertical drives, and conveyors

Integrator Ceratec Group:

  • This family-owned company, with more than 35 years of experience, operates in 27 countries across 5 continents and maintains more than 20,000 m² of state-of-the-art facilities.
  • Headquarters: Ploegsteert, Belgium
  • Industry: Automation, material handling, intralogistics, electrical engineering, heavy-duty ceramic solutions
  • Number of Employees: 550
  • High grid quality, therefore no need for power feedback
  • No braking resistances, as their heat output must be compensated for in the cold storage facility
  • High utilization rate
  • Fast return on investment
  • The entire electrical engineering project was carried out jointly by Ceratec and SEW-EURODRIVE
  • The software was developed on-site and tested at the SEW-EURODRIVE Innovation Center in Belgium
  • The hardware connections for all control cabinets were inspected and approved by SEW-EURODRIVE at Ceratec’s facility prior to startup
  • Close collaboration and open discussions with NewCold Engineering throughout the project
  • Fast return on investment through downsizing of the electrical installation—the peak power per storage/retrieval system is reduced by more than a factor of 5 (from 140 kW to 25 kW)
  • Increased uptime, as the simultaneous operation factor of the storage/retrieval systems is increased to 100%
  • High power quality and an energy-saving solution through internal energy recovery—energy is used where it is generated
  • Prevention of mechanical damage to the storage/retrieval system through electrical braking in the event of a fault
  • Cable vibration during shuttle retraction and extension in the ASRS is minimized thanks to improved connection of the distance encoders
  • Operational risks are reduced in compliance with standards thanks to fully integrated safety technology in the inverter that can be controlled via PROFIsafe
  • Quick startup thanks to thorough preparation prior to order picking and the configurable MOVIKIT®® software modules
  • Shorter safety approval process thanks to configurable safety option cards
  • Reduced qualification effort for maintenance due to consistent device behavior within the MOVI-C® automation modular system

By activating this video, Youtube will transfer data to the USA. More in our privacy policy.

A company with extensive expertise

NewCold boasts market-leading, in-house expertise in the design, engineering, development and operation of cutting-edge automated cold storage facilities. This know-how comes from the successful development and operation of more than 20 automated storage facilities over the last 18 years. The implementation expertise offered by NewCold covers training, maintenance, operational support and planning. On-site integration work gets underway in plenty of time before the storage facility goes live. NewCold aims to offer leading food companies the best possible logistics experience for the cold chain.

The project in Rennes was a very special job for NewCold. It was the first time we had worked with energy storage units in storage/retrieval systems. Working with SEW-EURODRIVE, we implemented a solution for reducing peak power from the grid, which means that much smaller components can be used in the power infeed. The challenge was integrating the energy storage units into the storage and retrieval systems, but the outstanding cooperation between NewCold, Ceratec and SEW-EURODRIVE made that possible.
Patrick de Breet (NewCold, Senior Project Manager)

Storage/retrieval system:

  • parameterizable MOVI-C® CONTROLLER progressive UHX65A
  • MOVIKIT®StackerCrane and MultiAxisController software modules for optimized control of the storage/retrieval system and PowerMode for managing the storage capacitors
  • Tried-and-tested gearmotors with 7-series gear units and DR.. motors


Shuttle:

  • parameterizable MOVI-C® CONTROLLER standard UHX25
  • Power supply MOVI‑DPS® for intelligent power and energy management in mobile applications
  • Dynamic servo gearmotors with planetary gear units
  • Tried-and-tested gearmotors with 7-series gear units and DR.. motors
  • Tried-and-tested gearmotors with 7-series gear units and DR.. motors

MOVIMOT® advanced with an integrated, decentralized frequency inverter offers full flexibility for your application – an all-rounder for use in numerous smart logistics applications.








  • The standard solution for all materials handling applications
  • Suitable for a wide range of applications, from speed control to positioning
  • Inverter integration minimizes assembly work
  • High-performance connection to all standard communication systems
  • Diverse gear unit combinations for customized adaptation