We put all our passion for technology into developing the best solutions for our customers. Do you need advice about a specific application?

Contact us now
Customer: Südzucker AG

Plant engineer:
Westa Fördertechnik GmbH

Location:
Offstein (Germany)

Sector:
Foodstuffs

Application:
Drive technology for a sugar beet conveyor belt

Contact form Worldwide locations Contact information

By activating the zip code search, data is transferred to the USA by Google. For more information, see our privacy policy.

The project at a glance

  • Client: Südzucker AG
  • Equipment Manufacturer: Westa Materials Handling Technology GmbH
  • Location: Offstein (Germany)
  • Industry: Food
  • Application: Drive technology for a sugar beet conveyor belt

More information about Südzucker AG:

  • Employees (2019): 16,500
  • Headquarters: Mannheim
  • Major Shareholder: 56% of the capital is held by sugar beet farmers organized through the Süddeutsche Zuckerrübenverwertungs-Genossenschaft eG (SZVG).
  • Production: 4.7 million metric tons of sugar per year
  • Locations: International setup, 9 locations in Germany
  • 1883: The Offstein sugar factory is founded
  • 1920: The Offstein and Groß-Gerau sugar factories merge; the Interest Group of Southern German Sugar Factories is founded
  • 1926: The Süddeutsche Zucker-Aktiengesellschaft, Mannheim, is formed from the merger of five regional sugar companies
  • 1988: Süddeutsche Zucker-Aktiengesellschaft and Zuckerfabrik Franken GmbH merge to form Südzucker Aktiengesellschaft Mannheim/Ochsenfurt
  • 2001:Südzucker celebrates its 75th anniversary
  • 2015: Südzucker Aktiengesellschaft Mannheim/Ochsenfurt is renamed Südzucker AG

More information about Westa materials handling technology:

  • Manufacturer of materials handling technology systems and accessories for bulk and piece goods transport, the automotive industry, and the recycling industry
  • Employees (2019): 80
  • Headquarters: Göllheim
  • Founded: 1972
  • Production area: > 4,000 m2
  • Modernization (service retrofit) of a sugar beet conveyor belt as part of a partial upgrade of the production facilities
  • Increase in the system’s conveying capacity to a maximum of 1,100 metric tons per hour
  • Belt conveyor with a length of 132 meters
  • Absolute assurance of production reliability and service life
  • Use of food-grade lubricants
  • Two redundant drive units
    • One IE3 AC motor DRN.. each with a power rating of 200 kW and a soft start
    • Three-stage industrial gear unit, type X3KS20/HU/B (bevel-spur gear unit), with a rated torque of 90 kNm
    • Power reserve for reliable operation and extended service life
    • Two redundant drive units: in the event of a failure, operation can be switched to the second drive
    • Motors are interchangeable
  • Custom solutions
    • Maintenance-free and with fail-safety for axial fan for cooling
    • Temperature sensor in the gear unit
    • Food-grade gear oil
    • Food-grade grease for the motors’ groove ball bearings
  • Comprehensive Retrofit Service
    • Analysis and design of drive technology
    • Selection and mounting of suitable drive components
    • Responsive and reliable service
  • Increased sugar beet conveying capacity at the plant
  • High production reliability and process reliability during critical production periods
  • High redundancy and service life
  • Simplified maintenance and spare part inventory management

At Südzucker AG's Offstein factory, the annual sugar beet crop is transported along a central conveyor belt at a rate of up to 16 000 metric tons per day. Drive technology from SEW‑EURODRIVE was the equipment of choice for retrofitting this belt conveyor. Our customized solution combined redundant drive units with powerful motors and robust industrial gear units. We improved production reliability while also increasing the conveying capacity to as much as 11 000 metric tons of beet – and that's per hour!

We have installed a large number of drives from SEW‑EURODRIVE at the Offstein factory and, after years of positive experiences, SEW‑EURODRIVE has virtually become one of our house brands. When preparing a call for tenders, SEW‑EURODRIVE is one of our preferred suppliers. We use the company's motors and gear units for screw and belt conveyors along with many other drive applications at the factory.
Maximilian Krantz, responsible for process engineering at Südzucker
Even special requests are no problem. SEW‑EURODRIVE has thoroughly impressed us with both its range of products and its collaboration, so we'll continue working with the company in the future. It was absolutely clear which company we would be using for the drives, because we know from our decades of experience that we can always rely on the extremely long-lasting quality and rapid service of SEW‑EURODRIVE.
Mario Stolzenberg, a project manager at Westa Fördertechnik
When the people on both sides of the table are highly competent, work is enjoyable and everyone contributes their know-how, which ultimately delivers a great result.
Bernhard Lang, a sales engineer at SEW‑EURODRIVE

Between September and December, Südzucker AG's Offstein factory is extremely busy, processing the annual sugar beet crop by turning up to 16 000 metric tons of sugar beet into some 2000 metric tons of sugar and syrup each day. At the heart of the production facility is a conveyor belt that takes the sugar beet to the production process. In addition to preventing this component from breaking down at all costs, an overhaul of the belt conveyor was also essential.

Südzucker AG awarded the contract for the redesign work to Westa Fördertechnik from Göllheim, an expert in its field that has been a Südzucker supplier for many years. Right from the outset, everyone involved was aware of the particular challenge of this project. Availability and reliability were the top priorities. With a conveyor belt 132 meters long and the belt alone weighing nine metric tons, there were also numerous variables that could not be defined with any degree of precision – an additional headache.

Given these sensitive issues and the high level of production reliability required, only well-known, dependable suppliers were used. SEW‑EURODRIVE was the preferred partner for drive technology, in particular because of its long-lasting product quality, impressive reliability, rapid service and considerable experience with stationary conveyor lines the world over.

A drive design with a sufficient power reserve was first agreed on in consultation with SEW‑EURODRIVE. The calculated belt speed and the gear unit dimensioning were also increased to be on the safe side. Positive effects on the service life were an added bonus.

The final drive solution was geared entirely to reliable, uninterrupted sugar production. Not one but two motor-gear unit combinations are now flange-mounted on the conveyor belt – one to the right of the conveyor drum and one to the left. If one drive fails, Südzucker can simply switch to the other. Following a quick mechanical conversion of the pin coupling between gearmotor and conveyor drum, the sugar beet resumes its journey.

Each drive unit has an energy-efficient 200 kW fixed-speed IE3 DRN.. AC motor with soft-start function. Large X3KS2010/HU/B industrial gear units – designed for a nominal gear unit torque of 90 kNm – transfer the motors' torque to the conveyor belt, reducing a motor speed of 1489 min-1 to the conveyor belt's output speed of 33 min-1.

The three-stage bevel-helical gear units are largely identical but operate with different directions of rotation. The key design feature of our modified gear unit is that the motors have the same direction of rotation, which means they can simply be interchanged in an emergency. In addition to improved redundancy and availability, Südzucker also benefits from simplified warehousing thanks to identical spare parts.

The industrial gear units in use in Offstein convert high motor speeds into low belt speeds. The heat this process generates necessitates active cooling. We normally use oil-air coolers for such tasks, but that would be another component that could break down, so our experts opted for a special solution – a specifically optimized axial fan between motor and gear unit. Operating at the same speed as the motor, the maintenance-free fan is both simple and effective, with no need for a separate controller. Südzucker thus benefits from enhanced reliability and lower maintenance costs.

The axial fan was just one of several ingenious add-on solutions. We applied food-grade lubricants approved by Südzucker to the conveyor belt. This included the oil for the gear units and a special grease for the motors' grooved ball bearings. Also at the customer's request, we gave the gear unit its own integrated temperature sensor.

The reason why we're so flexible when it comes to such special measures is simple – we do virtually everything ourselves. Almost all production steps take place in-house – from gear unit production to motor winding – and we love making our customers happy, even in the case of challenging requirements like those of Südzucker in Offstein. Bring on the next sugar beet harvest!