We put all our passion for technology into developing the best solutions for our customers. Do you need advice about a specific application?

Contact us now
Customer: KraussMaffei Berstorff GmbH

Location:
Hannover (Germany)

Sector:
Tire industry

Application:
Two-roll calender

Contact form Worldwide locations Contact information

By activating the zip code search, data is transferred to the USA by Google. For more information, see our privacy policy.

Thanks to the hard work of the SEW staff on site and their willingness to explore new approaches with our team, we were able to develop a standardized SEW solution that allowed us to design cost-effective machines that can be delivered quickly. We collaborated with SEW-EURODRIVE to produce four-roll calenders, which are now being used worldwide.
Ulrich Schmager – Head of Engineering Rubber Technology
  • Location: Hanover (Germany)
  • Sector: Tire industry
  • Application: Two-roll calender
  • Power/torque
  • Reliable, robust solution
  • Standardized industrial gear units
  • Reduced purchase price thanks to lack of special designs
  • 4-stage X gear unit tailored to suit a variety of system characteristics (e.g. number of rolls) and torques.
  • DRN motors with a DUB (Diagnostic Unit Brake) function to monitor brake wear.
  • Our DRN motor offers a highly reliable safety function thanks to our integrated brake, which allows the calender rolls to be brought to a halt within 30 degrees in an emergency, even when running at full speed.
  • Standardized large gear units instead of special gear units

KraussMaffei Berstorff is synonymous worldwide with state-of-the-art extrusion solutions that retain their value. It can supply anything from individual extruders with appropriate dies to upstream and downstream components and automated system solutions. The largest production locations for the KraussMaffei Berstorff brand within the corporate group are Hanover, Munich and Haiyan (China). While the Hanover site mainly produces extrusion lines and systems for customers in the automotive and industrial chemicals industries, the site in Munich focuses on producing lines for customers in the construction sector.