Driven by a passion for technology, we develop the best solutions for our customers. Do you have a specific application and would like some advice?

Contact us now
Client: GEA

Location:
Belgium

industry:
Pharmaceutical Industry

Application:
Cleanroom

Contact form Worldwide locations Contact information

By activating the zip code search, data is transferred to the USA by Google. For more information, see our privacy policy.

GEA

Location: Belgium

Industry: Pharmaceutical Industry

Application: Cleanroom

• The software, open-loop control system, inverter, drive system, and energy transfer had to come from a single manufacturer.

• Implementation in a very confined space

• FA57BCMPZ71S Servo parallel-shaft helical gearmotor with 2 kW drive power

• Servo Bevel Geared Motor KA57BCMPZ71S with a power rating of 2 kW

• FA37BCMP63M parallel-shaft helical gearmotor

• Four KA19CMP50S servo bevel gearmotors

• All applications from a single source

• All requirements were met within a minimal footprint.

Especially for its medications, which are manufactured for heart and cancer treatments, this pharmaceutical company sets manufacturing standards that exceed industry norms as a matter of course. In addition, to meet the quality standards for these medications as specified by an FDA guideline, the human factor—as a source of contamination—had to be eliminated, necessitating a switch to fully automated production.

At the pharmaceutical company’s Belgian production facility, a new cleanroom area is currently being commissioned. A cleanroom? No! This consists of up to four mobile cleanrooms within the cleanroom itself. The idea originated in Hürth, near Cologne, from the experts at GEA Lyophil. Drawing on the extensive experience of GEA’s experts and the systems already in operation at this manufacturer, GEA was tasked with the challenge: “How can the process steps of an existing plant be expanded and integrated in such a way as to secure the site’s future for the next 10 to 20 years?”