• Our experts know your industry and its requirements.
  • Our global network ensures we are there wherever and whenever you need us.
  • We have the expertise and tools to provide optimum advice and support.
Contact us now
The benefits for you

Fast startup
Thanks to optimized usability, MOVISUITE® is designed for simple, intuitive operation.

Consistent
MOVISUITE® is the startup engineering software for the entire unit portfolio of the MOVI-C® modular automation system - from gear units to control systems.

Free of charge
The software is freely available on the homepage. There are no costs for its use.

Complete
The software package contains functions for drive startup as well as for visualization and programming.

Control technology Control cabinet technology Decentralized drive technology Drive technology

MOVISUITE®: Perfect for today – ready for tomorrow

It may sound too good to be true, but that's exactly what we set out to provide when developing customized solutions for your automation and engineering requirements. This is all the more important if such solutions are to make your day-to-day work easier and offer future-proof assistance for your planning and orders – support you can rely on for the long term.

With MOVISUITE® standard, all components of the MOVI-C® modular automation system can be configured, started up and monitored throughout, from control technology to inverters, motors and gear units.

NEW! MOVISUITE® compact, the new compact variant of the engineering software, is optimized for the inverter, i.e. from the actual drive train to the motor to the gear unit. MOVI-C® CONTROLLERS are not supported. This allows for a very fast installation time and a reduced need for hard disk capacity.

This saves resources, time and money.

At the same time, both variant of MOVISUITE® feature the “look and feel” and graphical user interfaces of a uniform and modern engineering software.

Contact form Worldwide locations Contact information

By activating the zip code search, data is transferred to the USA by Google. For more information, see our privacy policy.

Overview of MOVISUITE®:
Rapid engineering thanks to unique usability and optimized workflows

  • End-to-end engineering for all components in the MOVI‑C® modular automation system – from inverters to customer-specific drive technology
  • Rapid engineering thanks to unique usability and optimized workflows
  • User-friendly operation with a modern look and feel, plus state-of-the-art GUI technology
  • Simple accessibility thanks to homogenized engineering interfaces
  • Startup and parameterization of the MOVIDRIVE® modular, technology and system application inverters
  • State-of-the-art interactive design makes it quick and easy for users to familiarize themselves with the software
  • Optimized workflows for professional and occasional users
  • Intuitive handling of inverter functions such as manual mode and drive train startup
  • MOVIKIT® software module parameterization and diagnostics
  • Efficient data management
  • Integrated project management
  • Network scan and device display
  • Scope function
  • Electronic catalog for products from SEW‑EURODRIVE
  • Extensive context-sensitive help for users

MOVISUITE® standard:

  • Engineering and programming of all components of the MOVI-C® modular automation system including MOVI-C® CONTROLLER
  • Startup, parameterization, diagnostics and optimization of control cabinet technology and decentralized drive technology from the MOVI-C® modular automation system
  • Parameter setting and diagnostics of the MOVIKIT® software modules for MOVI-C® CONTROLLERS, control cabinet inverter and decentralized drive technology

NEW! The compact variant: MOVISUITE® compact:

  • Startup, parameterization, diagnostics and optimization of control cabinet inverters and decentralized drive technology from the MOVI-C® modular automation system
  • Parameter setting and diagnostics of the MOVIKIT® software modules for control cabinet inverters and decentralized drive technology
  • Quick Installation
  • Low demand for hard disk capacity

The MOVIRUN® software platform is designed to be a universal solution, meaning it runs on the entire controller portfolio, MOVI‑C® CONTROLLER (control cabinet technology) and MOVI‑C® FIELD CONTROLLER (decentralized field installations).

MOVIRUN® determines the type and version of the runtime system, that is to say how the commands are executed by the control technology, and at what speed. The MOVIRUN® flexible version makes it possible to use motion control functions ranging from simple to complex and to do so efficiently using graphical user interfaces.

Human-centered design is all about meeting the requirements that will ensure software is developed and designed around user needs, is geared towards people in generaland delivers the user experience of a state-of-the-art software package. These requirements are even described and laid down in a technical standard, specifically DIN ISO 9410-210. But what exactly are the stipulations behind this standard and its numerical code? Quite simply, they offer a definition that describes how to make software and user interfaces easier to use.

All development work should revolve around the person who will later have to work with the software. That's why most interdisciplinary teams of developers ideally like to begin by putting themselves in the shoes of users and considering questions such as: Who are the typical users? What do they want to achieve with the product? And what is the easiest way they can reach their objective?

After that, the initial prototypes are developed and subjected to thorough testing by potential users. This means any necessary optimizations can be quickly identified and put into practice. The goal throughout is to combine the highest possible level of user-friendliness and usability.

By activating this video, Youtube will transfer data to the USA. More in our privacy policy.

NEW – The compact variant MOVISUITE® compact:

Meet the new compact software version for your engineering:

MOVISUITE® compact – small space requirements – quick installation

By activating this video, Youtube will transfer data to the USA. More in our privacy policy.

Overview of the basic functions

In this video, we provide you with an overview of the basic functions of MOVISUITE®.

By activating this video, Youtube will transfer data to the USA. More in our privacy policy.

Starting up a drive train

In this video, we show you how to start up a drive train using MOVISUITE®.

By activating this video, Youtube will transfer data to the USA. More in our privacy policy.

In this video, we show you the controller optimization process and the settings for manual mode when using MOVISUITE®.

You can find more tutorials about MOVISUITE® here

Thanks to the preconfigured MOVIKIT® software modules, any startup process can be carried out quickly and easily. Areas of application are just as varied as the motion and drive tasks that drive technology has to complete in automation solutions – from speed control and positioning to controlling complex technology or machine modules. Users are guided intuitively through the user interface, the configuration process and diagnostic functions. The MOVIKIT® software modules are divided into different categories and are available for the various versions of the MOVIRUN® software platforms.

Find out more about MOVIKIT® Find out more about MOVIRUN®
Go to the free download

Quote

Motion control without the headaches Control cabinet strain reduction Modularity in the field Always on the move