In the hoisting gear of a crane, a parallel shaft gear unit is often used for the hoisting drive, in which the rope drum and the motor are arranged on the same gear side. Suitable drives have a larger center distance to allow a large rope drum to be placed on the output shaft. The new G..7 gear units from SEW-EURODRIVE have been specially developed for hoists and have an increased center distance.