We put all our passion for technology into developing the best solutions for our customers. Do you need advice about a specific application?

Contact us now
Customer: Vollack Gruppe

Plant engineer:
Stadtwerke Karlsruhe

Location:
Karlsruhe

Sector:
Construction industry

Application:
Photovoltaic system

Contact form Worldwide locations Contact information

By activating the zip code search, data is transferred to the USA by Google. For more information, see our privacy policy.

Customers support renewable energy generation

Why not combine the pleasant with the useful? This was what Karlsruhe-based construction service provider Vollack thought when it decided to install a visually attractive photovoltaic system on its premises. It worked with Stadtwerke Karlsruhe and SEW-EURODRIVE to draw up a plan, the results of which are something to behold.

Some of the cost of the three solar sails were covered by a special initative: For more than 15 years, committed customers of Stadtwerke Karlsruhe have had the opportunity to make a personal contribution to supporting renewable energy generation. "They pay an additional fee, and this helps finance particularly innovative projects," explains the responsible Managing Director of Stadtwerke Karlsruhe.

They pay an additional fee, and this helps finance particularly innovative projects.
Managing Director of Stadtwerke Karlsruhe

Our solution

To obtain the highest possible energy yield, our gearmotors enable the sails to follow the sun.When the wind reaches force seven, the gearmotors also ensure the sails turn out of the wind to expose as little area as possible.

A sensor was attached to the rear sail that measures the strength of the wind. There is also a wind direction sensor on the roof of the Vollack building. This data is transmitted continuously so that the sail can be moved if the wind direction changes.


Overview

More than just the experience we have gained, we also wanted to send a very visible message that will hopefully encourage others to integrate environmentally and climate-friendly energy technology into challenging architectural concepts.
Stadwerke Karlsruhe have an eye on the future