We put all our passion for technology into developing the best solutions for our customers. Do you need advice about a specific application?

Contact us now
Customer: Hawle Austria Group

Plant engineer:
Hörmann Logistik GmbH, Munich, Germany

Location:
Vöcklabruck, Austria

Sector:
intralogistics

Application:
storage/retrieval system

Contact form Worldwide locations Contact information

By activating the zip code search, data is transferred to the USA by Google. For more information, see our privacy policy.

However, in terms of energy efficiency, the Austrian company has achieved its greatest success to date through the use of Powercaps. Equipment manufacturer Hörmann Logistik and SEW‑EURODRIVE used Powercaps to create a power and energy management solution for the new, automated high-bay warehouse – a solution that reduces the power demand of the storage/retrieval systems by a factor of 7 to 10.

  • Client: Hawle Austria Group, Vöcklabruck, Austria
  • Application: Storage/retrieval system
  • Industry: manufacturing (valve manufacturer for water and wastewater systems)
  • Additional information about our client:
    • 1,300 employees
    • 12 subsidiaries and an international network of partners
    • A broad product range of shut-off, distribution, and control valves, as well as pipe fittings and pipe sections
  • System Integrator: Hörmann Logistik GmbH, Munich, Germany
  • Industry: Intralogistics
  • More information about our client:
    • 2,787 employees
    • 30 affiliated companies
    • 4 business segments: Automotive, Communication, Intralogistics, and Engineering

Practical use of renewable energy

  • New automated high-bay warehouse:
  • Warehouse height: 29 m
  • Number of aisles: 5
  • Total weight per storage/retrieval system: approx. 25 metric tons
  • Peak power requirement with standard grid-side planning: 60 to 70 kW per storage/retrieval system
  • Specified targets:
    • Significantly reduced peak power requirements
    • Improved energy efficiency
  • Energy and Power Management via Power and Energy Solutions
  • MOVI-C® modular automation system®
  • Double-layer capacitor modules (Powercaps)
  • Approx. 200 gearmotors (175 for materials handling technology and 20 for the storage/retrieval system).
  • MOVI-C® CONTROLLER progressive UHX65 with MOVIKIT® software module® StackerCrane
  • MOVIDRIVE® modular frequency inverters with MDP92A power supply module (25 kW) featuring regulated DC link voltage and MDA90A single-axis modules (100 A and 48 A) with integrated CSS31A safety cards
  • Green success story
  • Reduction in power peaks and total energy consumption
  • Savings of approximately 230,000 kilowatt-hours (kWh) per year (equivalent to the current consumption of 52 average households)
  • Positive ecological impact of the SEW drive solution for the storage/retrieval systems
  • Wide range of applications for power and energy management

Long-standing innovative partnership

Together with Hawle, Hörmann Logistik and SEW-EURODRIVE, a lot of work was carried out, calculated and simulated in advance. How much energy can be charged into the powercaps when the hoist moves from top to bottom? For which travel movements is a fully or half-charged energy storage unit sufficient? Which scenarios require additional current from the grid? These and many other questions had to be answered in terms of control technology. The complexity behind this intelligent power and energy management solution is hidden from the operator. "We are the pure beneficiaries of this technology. In some cases, we are even below forecasts in terms of supply power," says Johannes Kräutner. At Hawle, he was primarily responsible for the warehouse project. In his opinion, things could not have been better at all: “The working environment was good and everything was very quiet but still dynamic,” he concludes.

Comments from our customers

"The Powercaps are brilliant. In my opinion, this energy storage technology which keeps the energy close to the system has the potential to play a key part in reducing worldwide energy consumption."
Johannes Kräutner, plant engineer at E. Hawle Armaturenwerke GmbH
"By using this innovative energy management solution, we're saving 230 000 kilowatt hours per year. That's the same amount of electricity used by 52 average households."
Andreas Bamberger, energy manager at E. Hawle Armaturenwerke GmbH
"We want to promote Power and Energy Solutions by SEW‑EURODRIVE to a greater extent in the future, because it's an ideal way of leaving behind a green footprint, including when it comes to intralogistics applications in particular."
Bernd Nebel, automation technology project manager at Hörmann Logistik GmbH
"Right from the very first load tests, it was clear that we actually need relatively little power to complete the necessary number of pallet storage and retrieval operations."
Hermann Pichler, automation engineer at E. Hawle Armaturenwerke GmbH
"SEW-EURODRIVE and Hörmann have a long-standing innovation partnership. With combined expertise, we have already made major leaps several times, which have brought many benefits for our customers."
Bernd Nebel, automation technology project manager at Hörmann Logistik GmbH