We put all our passion for technology into developing the best solutions for our customers. Do you need advice about a specific application?

Contact us now
Customer: SMC

Location:
Spresiano (Province of Treviso)

Sector:
Mechanical engineering

Application:
Agitator for synthetic latex

Contact form Worldwide locations Contact information

By activating the zip code search, data is transferred to the USA by Google. For more information, see our privacy policy.

The project at a glance

SMC, from Spresiano (Province of Treviso) is a global manufacturer of production plants. It provides construction services as well as associated technical consulting and planning services. Its customers include leading companies from the chemicals, pharmaceuticals and food industry as well as the waste management and recycling sector. SMC developed special know-how in manufacturing plants that maximise productivity – with minimal actual costs for capital, energy, maintenance and downtime. Their eye for detail, new process solutions and the ability to provide special solutions for every requirement make the company a competent and reliable partner.

This challenge requires the selection of a reliable partner for drive technology. SEW-EURODRIVE has been supporting SMC in ambitious projects for 35 years. This cooperation is based on common principles, where the focus in on the customer: experienced sales engineers and technicians analyse the requirements together with the customer, identify the production characteristics and present customized solution proposals. As a global company, SEW-EURODRIVE can also provide quick, comprehensive and efficient service.

To manufacture this reactor, with its impressive figures and the high power requirement, SMC's primary focus was to ensure that the gear units provided fully met these requirements in every respect. Moreover, quick and efficient service had to be guaranteed in the event of an incident.

Thanks to our low-maintenance X series industrial gear units and our comprehensive know-how in drive technology, we were able to provide a matching and powerful drive solution. As a global company, we also provide comprehensive service.

Agitator for synthetic latex: The driving force is the X series gear unit

The reactor displays impressive figures: an internal volume of 110 cubic meters, a production capacity of 90 cubic meters per cycle, an inner diameter of 3.80 meters, a height of 10.30 meters and a total mass of 79 tonnes. Every reactor is equipped with a customized agitator. As the agitator unit is of particular importance for these kinds of dimensions and requirements, the decision was made to use a robust X series industrial gear unit from SEW-EURODRIVE. The latest technology was used to manufacture the gear wheel, for the heat treatment as well as for the mechanical processing and the robust housing for the industrial gear units used. Due to the high axial loads, the ambient conditions, the danger zone and the special customer requirements, SEW-EURODRIVE equipped the X series gear units (size 210) with a vertical mounting position and a reduction ratio of 44:1. They generate a nominal torque of 90,000 Nm.

Powerful and safe agitation thanks to special adaptations

The X series industrial gear units are ideal for heavy duty applications and are typically used in production processes. The robust and universal gear unit series can be optimally adjusted to the relevant application conditions thanks to finely stepped torque ratings. The universal modular system sets standards for availability and ensures an extremely broad range of application options. The accessories and the agitator drive's special equipment features guarantee the functionality and reliability of the energy transfer for operation in a potentially explosive atmosphere. The drive is included in Group II, Category 2, in line with Directive 94/9/EC, generally referred to as ATEX.

The following adaptations were made to the industrial gear units for use and operation in the reactor: